Part Number: RM48L952
Good morning everyone. I'm using the rm48l952 microcontroller to create an SPI link only in tx to an LCD display.
I use spi4 with DMA, and I can send data (uint16) correctly. The speed clock of SPI4 is 10Mhz.
My problem is that there are some glitches on the chip_select[0] signal, of about 20 ns.
These glitches occur between the end of the character (16 bits) and the beginning of the next. Is it possible to eliminate these glitches,
so that the chip_select is lowered at the beginning of the frame and only raises at the end of the frame?
Regards, Luca.