Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
When using timer capture mode with two pins, it generates non-compiling code in syscfg/ti_msp_dl_config.c:
DL_TimerG_setCaptureCompareCtl(FAN_3_4_TACH_INST,
(DL_TIMER_CC_MODE_CAPTURE | DL_TIMER_CC_ZCOND_TRIG_RISE | DL_TIMER_CC_ACOND_TIMCLK | DL_TIMER_CC_CCOND_TRIG_RISE),
DL_TIMER_CC_1_INDEX);
The DL_TimerG_setCaptureCompareCtl function is defined as:
#define DL_TimerG_setCaptureCompareCtl DL_Timer_setCaptureCompareCtl
which refers to:
void DL_Timer_setCaptureCompareCtl(GPTIMER_Regs *gptimer, uint32_t ccMode,
uint32_t ccCondMask, DL_TIMER_CC_INDEX ccIndex);
This function has 4 arguments, but sysconfig tool generates a function call with 3 arguments only (merging ccMode and ccCondMask)
This is very annoying as in CCS studio the code gets auto generated everytime and therefor it never compiles rendering the whole CCS Studio unusable.