Part Number: LP-MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG, MSPM0L1306
1. I am working on using the LP-MSPM0L1306 EVM board. The board comes with blink led example which uses the 4MHz MFCLK. I am trying to use the sample example code but need to change the clock frequency to 32MHz clock instead of the 4MHz MFCLK, how can i accommodate this change?
2. I also need to know if the board can be flashed using the USB cable provided or does it need a standalone debugger for flashing?
3. what are the steps for using the usb cable for flashing?
4. what are the connections required for using a standalone debugger?