This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU with parallel interface

Hi team, 

     Is there any MCU available with parallel interface?

With Regards,

Jananni Sa

  • Hello Jananni,

    What sort of device are you trying to interface with? We have a device with a Universal Parallel Port (uPP) and devices with External Memory Interfaces (EMIF), can you clarify what your end application is for this?

    Best regards,

    Omer Amir

  • Hi Omer Amir,

      I want a MCU with serial interface like SPI/I2C to interface with RTC and a parallel interface to interface to a bus of width 4 bits. This MCU is integrated in a PCB of Dimension 16 x 10 mm. So, the MCU we are choosing should be less than this dimension also if RTC is integrated in the MCU it will be better, even it is not integrated it is also fine.

    With Regards,

    Jananni Sa

  • I want a MCU with serial interface like SPI/I2C to interface

    Nearly all devices have this, you can look at the C2000 Peripherals Guide for more details.

    a parallel interface to interface to a bus of width 4 bits

    What is the intention of this? Are you trying to interface with external memory such as by using EMIF, or something like uPP instead?

    This MCU is integrated in a PCB of Dimension 16 x 10 mm.

    Once you narrow down to a few devices based on peripherals, you can refer to the device datasheet "Mechanical, Packaging, and Orderable Information" section for size details.