This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Errata : CPU_ERR_01

Part Number: MSPM0G3507

Hi, 

I'm using driverlib in part. Are the following issues addressed by the latest driverlib currently available?

Errata : CPU_ERR_01

Title: CPU cache content can get corrupted

Revision : B

Details "Cache corruption can occur when switching between accessing Main flash memory, and other memory regions such as NONMAIN or Calibration data areas."

Workaround

Use the following procedure to access areas outside main memory safely:

1. Disable the cache by setting CTL.ICACHE to "0".

2. Perform needed access to memory area.

3. Re-enable cache by setting CTL.ICACHE to "1

Also related to this problem, I couldn't find where the calibration data area was.

In particular, I would like to check whether the address of the calibration data for the built-in thermometer used by driverlib is correct.

Related function :

dl_sysctl_mspm0g1x0x_g3x0x.h

DL_SYSCTL_getTempCalibrationConstant