Other Parts Discussed in Thread: TDA4VM
Hi,
I am using TDA4VM (J721E) board with SDK 09_00_00_00.
I have been using the board remotely, with ssh from my computer (as instructed in documentation https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-edgeai/TDA4VM/09_00_00/exports/docs/devices/TDA4VM/linux/getting_started.html ). But now I am getting "ssh: connect to host 192.168.0.53 port 22: Connection refused" error. What is the reason? I can ping to the board's IP but could not establish ssh session. Sometimes I am able to connect through ssh but it gets disconnected abruptly. It is a confusing behavior as it never happened in the past but it is happening now persistently.
P.S. I can ping from my computer to the board but when I do the same from terminal of board, it is random, sometimes ping is established but sometimes there is very large delay. I observed that whenever there is smooth ping from board to my system, I can establish ssh swiftly from my system to board and if delay comes in ping from board to my system the ssh session is exited.
Thanks and regards,
Sourabh