Part Number: LP-MSPM0L1306
#include "ti_msp_dl_config.h"
unsigned long count_timer = 0;
extern volatile uint32_t interruptVectors[];
int main(void)
{
SYSCFG_DL_init();
DL_SYSCTL_enableSleepOnExit();
NVIC_EnableIRQ(GPIO_SWITCHES_INT_IRQN);
NVIC_EnableIRQ(COMPARE_0_INST_INT_IRQN);
NVIC_EnableIRQ(TIMER_0_INST_INT_IRQN);
count_timer = 1500;
while (1) {
__WFI();
}
}
void GROUP1_IRQHandler(void)
{
uint32_t gpioA = DL_GPIO_getEnabledInterruptStatus
(GPIO_SWITCHES_PIN_18_PIN);
if ((gpioA & GPIO_SWITCHES_PIN_18_PIN) ==
GPIO_SWITCHES_PIN_18_PIN)
{
if (DL_GPIO_readPins(GPIO_SWITCHES_PORT, GPIO_SWITCHES_PIN_18_PIN ))
{
DL_TimerG_startCounter(COMPARE_0_INST);
DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN);
DL_GPIO_disableInterrupt(GPIOA, GPIO_SWITCHES_PIN_18_PIN);
}
DL_GPIO_clearInterruptStatus(GPIOA, GPIO_SWITCHES_PIN_18_PIN);
}
}
void COMPARE_0_INST_IRQHandler(void)
{
switch (DL_TimerG_getPendingInterrupt(COMPARE_0_INST)) {
case DL_TIMER_IIDX_ZERO:
if(count_timer>0)
{
count_timer = count_timer-1;
}
DL_TimerG_stopCounter(COMPARE_0_INST);
if (count_timer == 0)
{
DL_GPIO_clearPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN);
DL_GPIO_enableInterrupt(GPIOA, GPIO_SWITCHES_PIN_18_PIN);
count_timer = 1500;
}else if (count_timer > 0)
{
DL_TimerG_startCounter(COMPARE_0_INST);
}
break;
default:
break;
}
}
The intent of the code is that after detecting a GPIO interrupt, it starts a timer and repeats the timer operation for the set value of "count_timer",
and when "count_timer" reaches 0, the LED lights up. However, at this time, I would like to disable GPIO interrupts while repeating the timer operation.
However, there are some conditions in which the above code does not work properly.
After the timer starts operating (at this time, pin 18 is Low), before "count_timer" reaches 0, set the input of pin 18 to High again,
and if you continue to set it High until "count_timer" reaches 0, "count_timer" The moment it becomes 0 and DL_GPIO_enableInterrupt() is entered, another interrupt will occur and the timer will start working.
It seems that when DL_GPIO_enableInterrupt() operates, a pending GPIO interrupt is entered and a Timer interrupt is also entered.
When changing from disabling interrupts to enabling interrupts, how can I prevent pending interrupts from running and have interrupt triggers detected after enabling interrupts?
Are there any other settings required besides DL_GPIO_disableInterrupt() and DL_GPIO_enableInterrupt()?