Other Parts Discussed in Thread: BQ79616, USB2ANY
how can I get the code to read data from BQ79616 BMS through msp432e microcontroller can you please help me
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Meron,
I will need a bit more information. Could you please elaborate on the difficulties you are having? Software, hardware, device compatibility check, command protocol, etc. Are you using an EVM? Are you having issues with one particular section of code, or is code not working at all? Is this an issue primarily with the MCU or the BQ79616? If so, what leads you to believe this?
For general software information, please see the Software Design Guide: BQ79616-Q1 Software Design Reference (Rev. B) (ti.com).
Best,
Andria
yea i am using EVM and all the code is not working can not read any data from 79616 i was trying to check using logic analyzer but i don't know why. Below is my main code There is only one 79616 development board in the test. Please help me, thank you
#include <bq79616.h>
#include "string.h"
#include "sci.h"
#include "rti.h"
#include "gio.h"
#include "datatypes.h"
//GLOBAL VARIABLES (use these to avoid stack overflows by creating too many function variables)
//avoid creating variables/arrays in functions, or you will run out of stack space quickly
BYTE response_frame2[(MAXBYTES+6)*TOTALBOARDS]; //response frame to be used by every read
BYTE fault_frame[39*TOTALBOARDS]; //hold fault frame if faults are printed
int currentBoard = 0;
int currentCell = 0;
BYTE bReturn = 0;
int bRes = 0;
int count = 10000;
BYTE bBuf[8];
uint8 pFrame[64];
uint16 wCRC = 0;
uint16 wCRC16 = 0;
int crc_i = 0;
static volatile unsigned int delayval = 0; //for delayms and delayus functions
extern int UART_RX_RDY;
extern int RTI_TIMEOUT;
//******
//PINGS
//******
void Wake79616(void) {
sciREG->GCR1 &= ~(1U << 7U); // put SCI into reset
sciREG->PIO0 &= ~(1U << 2U); // disable transmit function - now a GPIO
sciREG->PIO3 &= ~(1U << 2U); // set output to low
delayus(2500); // WAKE ping = 2ms to 2.5ms
sciInit();
sciSetBaudrate(sciREG, BAUDRATE);
}
void SD79616(void) {
sciREG->GCR1 &= ~(1U << 7U); // put SCI into reset
sciREG->PIO0 &= ~(1U << 2U); // disable transmit function - now a GPIO
sciREG->PIO3 &= ~(1U << 2U); // set output to low
delayus(9000); // SD ping = 7ms to 10ms
sciInit();
sciSetBaudrate(sciREG, BAUDRATE);
}
void StA79616(void) {
sciREG->GCR1 &= ~(1U << 7U); // put SCI into reset
sciREG->PIO0 &= ~(1U << 2U); // disable transmit function - now a GPIO
sciREG->PIO3 &= ~(1U << 2U); // set output to low
delayus(250); // StA ping = 250us to 300us
sciInit();
sciSetBaudrate(sciREG, BAUDRATE);
}
void HWRST79616(void) {
sciREG->GCR1 &= ~(1U << 7U); // put SCI into reset
sciREG->PIO0 &= ~(1U << 2U); // disable transmit function - now a GPIO
sciREG->PIO3 &= ~(1U << 2U); // set output to low
delayus(36000); // StA ping = 36ms
sciInit();
sciSetBaudrate(sciREG, BAUDRATE);
}
//**********
//END PINGS
//**********
//**********************
//AUTO ADDRESS SEQUENCE
//**********************
void AutoAddress()
{
//DUMMY WRITE TO SNCHRONIZE ALL DAISY CHAIN DEVICES DLL (IF A DEVICE RESET OCCURED PRIOR TO THIS)
WriteReg(0, OTP_ECC_DATAIN1, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN2, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN3, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN4, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN5, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN6, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN7, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN8, 0X00, 1, FRMWRT_ALL_W);
//ENABLE AUTO ADDRESSING MODE
WriteReg(0, CONTROL1, 0X01, 1, FRMWRT_ALL_W);
//SET ADDRESSES FOR EVERY BOARD
for(currentBoard=0; currentBoard<TOTALBOARDS; currentBoard++)
{
WriteReg(0, DIR0_ADDR, currentBoard, 1, FRMWRT_ALL_W);
}
WriteReg(0, COMM_CTRL, 0x02, 1, FRMWRT_ALL_W); //set everything as a stack device first
if(TOTALBOARDS==1) //if there's only 1 board, it's the base AND top of stack, so change it to those
{
WriteReg(0, COMM_CTRL, 0x01, 1, FRMWRT_SGL_W);
}
else //otherwise set the base and top of stack individually
{
WriteReg(0, COMM_CTRL, 0x00, 1, FRMWRT_SGL_W);
WriteReg(TOTALBOARDS-1, COMM_CTRL, 0x03, 1, FRMWRT_SGL_W);
}
//SYNCRHONIZE THE DLL WITH A THROW-AWAY READ
ReadReg(0, OTP_ECC_DATAIN1, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN2, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN3, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN4, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN5, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN6, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN7, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN8, response_frame2, 1, 0, FRMWRT_ALL_R);
/*//OPTIONAL: read back all device addresses
for(currentBoard=0; currentBoard<TOTALBOARDS; currentBoard++)
{
ReadReg(currentBoard, DIR0_ADDR, response_frame2, 1, 0, FRMWRT_SGL_R);
printf("board %d\n",response_frame2[4]);
}*/
//RESET ANY COMM FAULT CONDITIONS FROM STARTUP
WriteReg(0, FAULT_RST2, 0x03, 1, FRMWRT_ALL_W);
return;
}
//**************************
//END AUTO ADDRESS SEQUENCE
//**************************
//************************
//WRITE AND READ FUNCTIONS
//************************
//FORMAT WRITE DATA, SEND TO
//BE COMBINED WITH REST OF FRAME
int WriteReg(BYTE bID, uint16 wAddr, uint64 dwData, BYTE bLen, BYTE bWriteType) {
// device address, register start address, data bytes, data length, write type (single, broadcast, stack)
bRes = 0;
memset(bBuf,0,sizeof(bBuf));
switch (bLen) {
case 1:
bBuf[0] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 1, bWriteType);
break;
case 2:
bBuf[0] = (dwData & 0x000000000000FF00) >> 8;
bBuf[1] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 2, bWriteType);
break;
case 3:
bBuf[0] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[1] = (dwData & 0x000000000000FF00) >> 8;
bBuf[2] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 3, bWriteType);
break;
case 4:
bBuf[0] = (dwData & 0x00000000FF000000) >> 24;
bBuf[1] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[2] = (dwData & 0x000000000000FF00) >> 8;
bBuf[3] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 4, bWriteType);
break;
case 5:
bBuf[0] = (dwData & 0x000000FF00000000) >> 32;
bBuf[1] = (dwData & 0x00000000FF000000) >> 24;
bBuf[2] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[3] = (dwData & 0x000000000000FF00) >> 8;
bBuf[4] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 5, bWriteType);
break;
case 6:
bBuf[0] = (dwData & 0x0000FF0000000000) >> 40;
bBuf[1] = (dwData & 0x000000FF00000000) >> 32;
bBuf[2] = (dwData & 0x00000000FF000000) >> 24;
bBuf[3] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[4] = (dwData & 0x000000000000FF00) >> 8;
bBuf[5] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 6, bWriteType);
break;
case 7:
bBuf[0] = (dwData & 0x00FF000000000000) >> 48;
bBuf[1] = (dwData & 0x0000FF0000000000) >> 40;
bBuf[2] = (dwData & 0x000000FF00000000) >> 32;
bBuf[3] = (dwData & 0x00000000FF000000) >> 24;
bBuf[4] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[5] = (dwData & 0x000000000000FF00) >> 8;
bBuf[6] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 7, bWriteType);
break;
case 8:
bBuf[0] = (dwData & 0xFF00000000000000) >> 56;
bBuf[1] = (dwData & 0x00FF000000000000) >> 48;
bBuf[2] = (dwData & 0x0000FF0000000000) >> 40;
bBuf[3] = (dwData & 0x000000FF00000000) >> 32;
bBuf[4] = (dwData & 0x00000000FF000000) >> 24;
bBuf[5] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[6] = (dwData & 0x000000000000FF00) >> 8;
bBuf[7] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 8, bWriteType);
break;
default:
break;
}
return bRes;
}
//GENERATE COMMAND FRAME
int WriteFrame(BYTE bID, uint16 wAddr, BYTE * pData, BYTE bLen, BYTE bWriteType) {
int bPktLen = 0;
uint8 * pBuf = pFrame;
memset(pFrame, 0x7F, sizeof(pFrame));
*pBuf++ = 0x80 | (bWriteType) | ((bWriteType & 0x10) ? bLen - 0x01 : 0x00); //Only include blen if it is a write; Writes are 0x90, 0xB0, 0xD0
if (bWriteType == FRMWRT_SGL_R || bWriteType == FRMWRT_SGL_W)
{
*pBuf++ = (bID & 0x00FF);
}
*pBuf++ = (wAddr & 0xFF00) >> 8;
*pBuf++ = wAddr & 0x00FF;
while (bLen--)
*pBuf++ = *pData++;
bPktLen = pBuf - pFrame;
wCRC = CRC16(pFrame, bPktLen);
*pBuf++ = wCRC & 0x00FF;
*pBuf++ = (wCRC & 0xFF00) >> 8;
bPktLen += 2;
//THIS SEEMS to occasionally drop bytes from the frame. Sometimes is not sending the last frame of the CRC.
//(Seems to be caused by stack overflow, so take precautions to reduce stack usage in function calls)
sciSend(sciREG, bPktLen, pFrame);
return bPktLen;
}
//GENERATE READ COMMAND FRAME AND THEN WAIT FOR RESPONSE DATA (INTERRUPT MODE FOR SCIRX)
int ReadReg(BYTE bID, uint16 wAddr, BYTE * pData, BYTE bLen, uint32 dwTimeOut,
BYTE bWriteType) {
// device address, register start address, byte frame pointer to store data, data length, read type (single, broadcast, stack)
bRes = 0;
count = 1000000; //timeout after this many attempts
if (bWriteType == FRMWRT_SGL_R) {
ReadFrameReq(bID, wAddr, bLen, bWriteType);
memset(pData, 0, sizeof(pData));
sciEnableNotification(sciREG, SCI_RX_INT);
sciReceive(sciREG, bLen + 6, pData);
while(UART_RX_RDY == 0U && count>0) count--; /* Wait */
UART_RX_RDY = 0;
bRes = bLen + 6;
} else if (bWriteType == FRMWRT_STK_R) {
bRes = ReadFrameReq(bID, wAddr, bLen, bWriteType);
memset(pData, 0, sizeof(pData));
sciEnableNotification(sciREG, SCI_RX_INT);
sciReceive(sciREG, (bLen + 6) * (TOTALBOARDS - 1), pData);
while(UART_RX_RDY == 0U && count>0) count--; /* Wait */
UART_RX_RDY = 0;
bRes = (bLen + 6) * (TOTALBOARDS - 1);
} else if (bWriteType == FRMWRT_ALL_R) {
bRes = ReadFrameReq(bID, wAddr, bLen, bWriteType);
memset(pData, 0, sizeof(pData));
sciEnableNotification(sciREG, SCI_RX_INT);
sciReceive(sciREG, (bLen + 6) * TOTALBOARDS, pData);
while(UART_RX_RDY == 0U && count>0) count--; /* Wait */
UART_RX_RDY = 0;
bRes = (bLen + 6) * TOTALBOARDS;
} else {
bRes = 0;
}
// //CHECK IF CRC IS CORRECT
// for(crc_i=0; crc_i<bRes; crc_i+=(bLen+6))
// {
// if(CRC16(&pData[crc_i], bLen+6)!=0)
// {
// printf("BAD CRC\n");
// }
// }
return bRes;
}
int ReadFrameReq(BYTE bID, uint16 wAddr, BYTE bByteToReturn, BYTE bWriteType) {
bReturn = bByteToReturn - 1;
if (bReturn > 127)
return 0;
return WriteFrame(bID, wAddr, &bReturn, 1, bWriteType);
}
// CRC16 TABLE
// ITU_T polynomial: x^16 + x^15 + x^2 + 1
const uint16 crc16_table[256] = { 0x0000, 0xC0C1, 0xC181, 0x0140, 0xC301,
0x03C0, 0x0280, 0xC241, 0xC601, 0x06C0, 0x0780, 0xC741, 0x0500, 0xC5C1,
0xC481, 0x0440, 0xCC01, 0x0CC0, 0x0D80, 0xCD41, 0x0F00, 0xCFC1, 0xCE81,
0x0E40, 0x0A00, 0xCAC1, 0xCB81, 0x0B40, 0xC901, 0x09C0, 0x0880, 0xC841,
0xD801, 0x18C0, 0x1980, 0xD941, 0x1B00, 0xDBC1, 0xDA81, 0x1A40, 0x1E00,
0xDEC1, 0xDF81, 0x1F40, 0xDD01, 0x1DC0, 0x1C80, 0xDC41, 0x1400, 0xD4C1,
0xD581, 0x1540, 0xD701, 0x17C0, 0x1680, 0xD641, 0xD201, 0x12C0, 0x1380,
0xD341, 0x1100, 0xD1C1, 0xD081, 0x1040, 0xF001, 0x30C0, 0x3180, 0xF141,
0x3300, 0xF3C1, 0xF281, 0x3240, 0x3600, 0xF6C1, 0xF781, 0x3740, 0xF501,
0x35C0, 0x3480, 0xF441, 0x3C00, 0xFCC1, 0xFD81, 0x3D40, 0xFF01, 0x3FC0,
0x3E80, 0xFE41, 0xFA01, 0x3AC0, 0x3B80, 0xFB41, 0x3900, 0xF9C1, 0xF881,
0x3840, 0x2800, 0xE8C1, 0xE981, 0x2940, 0xEB01, 0x2BC0, 0x2A80, 0xEA41,
0xEE01, 0x2EC0, 0x2F80, 0xEF41, 0x2D00, 0xEDC1, 0xEC81, 0x2C40, 0xE401,
0x24C0, 0x2580, 0xE541, 0x2700, 0xE7C1, 0xE681, 0x2640, 0x2200, 0xE2C1,
0xE381, 0x2340, 0xE101, 0x21C0, 0x2080, 0xE041, 0xA001, 0x60C0, 0x6180,
0xA141, 0x6300, 0xA3C1, 0xA281, 0x6240, 0x6600, 0xA6C1, 0xA781, 0x6740,
0xA501, 0x65C0, 0x6480, 0xA441, 0x6C00, 0xACC1, 0xAD81, 0x6D40, 0xAF01,
0x6FC0, 0x6E80, 0xAE41, 0xAA01, 0x6AC0, 0x6B80, 0xAB41, 0x6900, 0xA9C1,
0xA881, 0x6840, 0x7800, 0xB8C1, 0xB981, 0x7940, 0xBB01, 0x7BC0, 0x7A80,
0xBA41, 0xBE01, 0x7EC0, 0x7F80, 0xBF41, 0x7D00, 0xBDC1, 0xBC81, 0x7C40,
0xB401, 0x74C0, 0x7580, 0xB541, 0x7700, 0xB7C1, 0xB681, 0x7640, 0x7200,
0xB2C1, 0xB381, 0x7340, 0xB101, 0x71C0, 0x7080, 0xB041, 0x5000, 0x90C1,
0x9181, 0x5140, 0x9301, 0x53C0, 0x5280, 0x9241, 0x9601, 0x56C0, 0x5780,
0x9741, 0x5500, 0x95C1, 0x9481, 0x5440, 0x9C01, 0x5CC0, 0x5D80, 0x9D41,
0x5F00, 0x9FC1, 0x9E81, 0x5E40, 0x5A00, 0x9AC1, 0x9B81, 0x5B40, 0x9901,
0x59C0, 0x5880, 0x9841, 0x8801, 0x48C0, 0x4980, 0x8941, 0x4B00, 0x8BC1,
0x8A81, 0x4A40, 0x4E00, 0x8EC1, 0x8F81, 0x4F40, 0x8D01, 0x4DC0, 0x4C80,
0x8C41, 0x4400, 0x84C1, 0x8581, 0x4540, 0x8701, 0x47C0, 0x4680, 0x8641,
0x8201, 0x42C0, 0x4380, 0x8341, 0x4100, 0x81C1, 0x8081, 0x4040 };
uint16 CRC16(BYTE *pBuf, int nLen) {
uint16 wCRC = 0xFFFF;
int i;
for (i = 0; i < nLen; i++) {
wCRC ^= (*pBuf++) & 0x00FF;
wCRC = crc16_table[wCRC & 0x00FF] ^ (wCRC >> 8);
}
return wCRC;
}
//****************************
//END WRITE AND READ FUNCTIONS
//****************************
//************************
//MISCELLANEOUS FUNCTIONS
//************************
BOOL GetFaultStat() {
if (!gioGetBit(gioPORTA, 0))
return 0;
return 1;
}
void delayus(uint16 us) {
if (us == 0)
return;
else
{
//CHANGE THE INTERRUPT COMPARE VALUES (PERIOD OF INTERRUPT)
//Setup compare 0 value.
rtiREG1->CMP[0U].COMPx = 10*us; //10 ticks of clock per microsecond, so multiply by 10
//Setup update compare 0 value.
rtiREG1->CMP[0U].UDCPx = 10*us;
//ENABLE THE NOTIFICATION FOR THE PERIOD WE SET
rtiEnableNotification(rtiNOTIFICATION_COMPARE0);
//START THE COUNTER
rtiStartCounter(rtiCOUNTER_BLOCK0);
//WAIT IN LOOP UNTIL THE INTERRUPT HAPPENS (HAPPENS AFTER THE PERIOD WE SET)
//WHEN INTERRUPT HAPPENS, RTI_NOTIFICATION GETS SET TO 1 IN THAT INTERRUPT
//GO TO notification.c -> rtiNotification() to see where RTI_TIMEOUT is set to 1
while(RTI_TIMEOUT==0);
//RESET THE VARIABLE TO 0, FOR THE NEXT TIME WE DO A DELAY
RTI_TIMEOUT = 0;
//DISABLE THE INTERRUPT NOTIFICATION
rtiDisableNotification(rtiNOTIFICATION_COMPARE0);
//STOP THE COUNTER
rtiStopCounter(rtiCOUNTER_BLOCK0);
//RESET COUNTER FOR THE NEXT TIME WE DO A DELAY
rtiResetCounter(rtiCOUNTER_BLOCK0);
}
}
void delayms(uint16 ms) {
if (ms == 0)
return;
else
{
rtiREG1->CMP[0U].COMPx = 10000*ms;
rtiREG1->CMP[0U].UDCPx = 10000*ms;
rtiEnableNotification(rtiNOTIFICATION_COMPARE0);
rtiStartCounter(rtiCOUNTER_BLOCK0);
while(RTI_TIMEOUT==0);
RTI_TIMEOUT = 0;
rtiDisableNotification(rtiNOTIFICATION_COMPARE0);
rtiStopCounter(rtiCOUNTER_BLOCK0);
rtiResetCounter(rtiCOUNTER_BLOCK0);
}
}
void ResetAllFaults(BYTE bID, BYTE bWriteType)
{
int printf(const char *format, ...);
//BROADCAST INCLUDES EXTRA FUNCTIONALITY TO OVERWRITE THE CUST_CRC WITH THE CURRENT SETTINGS
if(bWriteType==FRMWRT_ALL_W)
{
//READ THE CALCULATED CUSTOMER CRC VALUES
ReadReg(0, CUST_CRC_RSLT_HI, fault_frame, 2, 0, FRMWRT_ALL_R);
//OVERWRITE THE CRC OF EVERY BOARD IN THE STACK WITH THE CORRECT CRC
for(currentBoard=0; currentBoard<TOTALBOARDS; currentBoard++)
{
//THE RETURN FRAME STARTS WITH THE HIGHEST BOARD FIRST, SO THIS WILL WRITE THE HIGHEST BOARD FIRST
WriteReg(TOTALBOARDS-currentBoard-1, CUST_CRC_HI, fault_frame[currentBoard*8+4] << 8 | fault_frame[currentBoard*8+5], 2, FRMWRT_SGL_W);
}
//NOW CLEAR EVERY FAULT
WriteReg(0, FAULT_RST1, 0xFFFF, 2, FRMWRT_ALL_W);
}
else if(bWriteType==FRMWRT_SGL_W)
{
WriteReg(bID, FAULT_RST1, 0xFFFF, 2, FRMWRT_SGL_W);
}
else if(bWriteType==FRMWRT_STK_W)
{
WriteReg(0, FAULT_RST1, 0xFFFF, 2, FRMWRT_STK_W);
}
else
{
printf("ERROR: ResetAllFaults bWriteType incorrect\n");
}
}
void MaskAllFaults(BYTE bID, BYTE bWriteType)
{
int printf(const char *format, ...);
if(bWriteType==FRMWRT_ALL_W)
{
WriteReg(0, FAULT_MSK1, 0xFFFF, 2, FRMWRT_ALL_W);
}
else if(bWriteType==FRMWRT_SGL_W)
{
WriteReg(bID, FAULT_MSK1, 0xFFFF, 2, FRMWRT_SGL_W);
}
else if(bWriteType==FRMWRT_STK_W)
{
WriteReg(0, FAULT_MSK1, 0xFFFF, 2, FRMWRT_STK_W);
}
else
{
printf("ERROR: MaskAllFaults bWriteType incorrect\n");
}
}
void PrintAllFaults(BYTE bID, BYTE bWriteType)
{
int printf(const char *format, ...);
//PRINT 39 REGISTERS STARTING FROM FAULT_SUMMARY (INCLUDES RESERVED REGISTERS)
printf("\n");
currentBoard = 0;
currentCell = 0;
memset(fault_frame,0,sizeof(fault_frame));
if(bWriteType==FRMWRT_ALL_R)
{
ReadReg(0, FAULT_SUMMARY, fault_frame, 39, 0, FRMWRT_ALL_R);
for(currentBoard = 0; currentBoard<TOTALBOARDS; currentBoard++)
{
printf("BOARD %d FAULTS:\t",TOTALBOARDS-currentBoard);
for(currentCell = 0; currentCell<39; currentCell++)
{
printf("%02x ",fault_frame[(currentBoard*(39+6))+4+currentCell]);
}
printf("\n");
}
}
else if(bWriteType==FRMWRT_SGL_R)
{
ReadReg(bID, FAULT_SUMMARY, fault_frame, 39, 0, FRMWRT_SGL_R);
printf("BOARD %d FAULTS:\t",bID);
for(currentCell = 0; currentCell<39; currentCell++)
{
printf("%02x ",fault_frame[4+currentCell]);
}
printf("\n");
}
else if(bWriteType==FRMWRT_STK_R)
{
ReadReg(0, FAULT_SUMMARY, fault_frame, 39, 0, FRMWRT_STK_R);
for(currentBoard = 0; currentBoard<(TOTALBOARDS-1); currentBoard++)
{
printf("BOARD %d FAULTS:\t",TOTALBOARDS-currentBoard);
for(currentCell = 0; currentCell<39; currentCell++)
{
printf("%02x ",fault_frame[(currentBoard*(39+6))+4+currentCell]);
}
printf("\n");
}
}
else
{
printf("ERROR: PrintAllFaults bWriteType incorrect\n");
}
printf("\n");
}
//RUN BASIC CELL BALANCING FOR ALL DEVICES
void RunCB()
{
//SET BALANCING TIMERS TO 30 s
WriteReg(0, CB_CELL16_CTRL, 0x0202020202020202, 8, FRMWRT_ALL_W); //cell 16-9 (8 byte max write)
WriteReg(0, CB_CELL8_CTRL, 0x0202020202020202, 8, FRMWRT_ALL_W); //cell 8-1
//SET DUTY CYCLE TO 10 s (default)
WriteReg(0, BAL_CTRL1, 0x01, 1, FRMWRT_ALL_W); //10s duty cycle
//OPTIONAL: SET VCBDONE THRESH TO 3V, AND OVUV_GO
WriteReg(0, VCB_DONE_THRESH, 0x08, 1, FRMWRT_ALL_W); //3V threshold (8*25mV + 2.8V)
WriteReg(0, OVUV_CTRL, 0x05, 1, FRMWRT_ALL_W); //round-robin and OVUV_GO
//START BALANCING
WriteReg(0, BAL_CTRL2, 0x03, 1, FRMWRT_ALL_W); //auto balance and BAL_GO
}
//RUN BASIC REVERSE ADDRESSING SEQUENCE
void ReverseAddressing()
{
//CHANGE BASE DEVICE DIRECTION
WriteReg(0, CONTROL1, 0x80, 1, FRMWRT_SGL_W);
//CHANGE REST OF STACK DIRECTION
WriteReg(0, CONTROL1, 0x80, 1, FRMWRT_REV_ALL_W);
//DO NORMAL AUTO ADDRESS SEQUENCE, BUT FOR DIR1_ADDR
//DUMMY WRITE TO SNCHRONIZE ALL DAISY CHAIN DEVICES DLL (IF A DEVICE RESET OCCURED PRIOR TO THIS)
WriteReg(0, OTP_ECC_DATAIN1, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN2, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN3, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN4, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN5, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN6, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN7, 0X00, 1, FRMWRT_ALL_W);
WriteReg(0, OTP_ECC_DATAIN8, 0X00, 1, FRMWRT_ALL_W);
//ENABLE AUTO ADDRESSING MODE, WHILE KEEPING REVERSE DIRECTION
WriteReg(0, CONTROL1, 0X81, 1, FRMWRT_ALL_W);
//SET ADDRESSES FOR EVERY BOARD (REVERSE DIRECTION)
for(currentBoard=0; currentBoard<TOTALBOARDS; currentBoard++)
{
WriteReg(0, DIR1_ADDR, currentBoard, 1, FRMWRT_ALL_W);
}
WriteReg(0, COMM_CTRL, 0x02, 1, FRMWRT_ALL_W); //set everything as a stack device first
if(TOTALBOARDS==1) //if there's only 1 board, it's the base AND top of stack, so change it to those
{
WriteReg(0, COMM_CTRL, 0x01, 1, FRMWRT_SGL_W);
}
else //otherwise set the base and top of stack individually
{
WriteReg(0, COMM_CTRL, 0x00, 1, FRMWRT_SGL_W);
WriteReg(TOTALBOARDS-1, COMM_CTRL, 0x03, 1, FRMWRT_SGL_W);
}
//SYNCRHONIZE THE DLL WITH A THROW-AWAY READ
ReadReg(0, OTP_ECC_DATAIN1, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN2, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN3, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN4, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN5, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN6, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN7, response_frame2, 1, 0, FRMWRT_ALL_R);
ReadReg(0, OTP_ECC_DATAIN8, response_frame2, 1, 0, FRMWRT_ALL_R);
////OPTIONAL: read back all device addresses
//for(currentBoard=0; currentBoard<TOTALBOARDS; currentBoard++)
//{
// ReadReg(currentBoard, DIR0_ADDR, response_frame2, 1, 0, FRMWRT_SGL_R);
// printf("board %d\n",response_frame2[4]);
//}
//RESET ANY COMM FAULT CONDITIONS FROM STARTUP
WriteReg(0, FAULT_RST2, 0x03, 1, FRMWRT_ALL_W);
}
//***************************
//END MISCELLANEOUS FUNCTIONS
//***************************
//EOF
Hi Meron,
Unfortunately, I cannot read through all your code and provide you with a comprehensive debug. To troubleshoot this issue, I recommend the following:
Best,
Andria