Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: uDMA Control Table as 32bit ?

Part Number: EK-TM4C123GXL

Why is the uDMA Control table declared as uint8_t and not as uint32_t in the Tivaware examples?

According to the datasheet the "registers" for the target address and so on are 32bit long.

  • Hi,

      I think the reason is that uDMA control table must be aligned to 1024 bytes. In order to satisfy this requirement, the software developer for the example uses the pragma DATA_ALIGN as follows to force the alignment. I suppose uint32_t can be used for pui8ControlTable[256] to achieve the same thing. 

    #pragma DATA_ALIGN(pui8ControlTable, 1024)
    uint8_t pui8ControlTable[1024];

    As a heads-up, I'm currently on vacation. Please expect delay in my response.