Hello,
Writing to the "ESM Low-Time Counter Preload" (ESMLTCPR) register using the routine bellow does not change it and neither the "ESM Low-Time Counter" (ESMLTCR) register, even when the ERROR pin status is forced to low.
/** @fn void esmSetCounterPreloadValue(uint32 value)
* @brief Set counter preload value
*
* @param[in] value - Counter preload value
*
* Set counter preload value.
*/
/* SourceId : ESM_SourceId_018 */
/* DesignId : ESM_DesignId_018 */
/* Requirements : HL_CONQ_ESM_SR11 */
void esmSetCounterPreloadValue(uint32 value)
{
/* USER CODE BEGIN (37) */
/* USER CODE END */
esmREG->LTCPR = value & 0xC000U;
/* USER CODE BEGIN (38) */
/* USER CODE END */
}
Best regards,