I final finish everything to a point where I can look at it and have follow the steps in the startup guide, but it won’t boot?
I get the below before renaming the files per the procedure:
- Rename tiboot3.bin to tiboot3-default.bin.
- Rename tiboot3-am62x-gp-evm.bin to tiboot3.bin.
I get nothing on terminal. Program
If I rename files back, I get on Terminal program.
U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
Is there something I missing (switches seem right)?