Part Number: AM2434
Other Parts Discussed in Thread: TMDS243EVM
Hello Champs,
HW: TMDS243EVM
SW: mcu_plus_sdk_am243x_08_06_00_48
Customer is debugging rmii pn demo load to cotex_R5,and run , EVM board two red led(LD22 andLD23) turn on.
Plug in the network cable, the network port light does not light up.
is there any manual to descript how to run PROFINET stack onTMDS243EVM ?
The board DeviceType is HSFS
-----------------------
SoC ID Header Info:
-----------------------
NumBlocks : 2
-----------------------
SoC ID Public ROM Info:
-----------------------
SubBlockId : 1
SubBlockSize : 26
DeviceName : am64x
DeviceType : HSFS
DMSC ROM Version : [0, 2, 0, 0]
R5 ROM Version : [0, 2, 0, 0]
-----------------------
SoC ID Secure ROM Info:
-----------------------
Sec SubBlockId : 2
Sec SubBlockSize : 166
Sec Prime : 0
Sec Key Revision : 0
Sec Key Count : 0
Sec TI MPK Hash : b018658ad99dc903c8c9bfb27b12751099920a042ad1dfea7b7ba57369f15546de285edde6a7b39a8bdc40a27b237f8fb1e57f245e80b929c1e28b024aa2ecc6
Sec Cust MPK Hash : ad0bc40b000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000
Sec Unique ID : 74168f15e6e9c7a03a4f895e168e9dd0ccd3949b53caecf327fd12450a89351e
demo path:C:\ti\mcu_plus_sdk_am243x_08_06_00_48\examples\industrial_comms\profinet_device_demo
log :
[APP] INFO: Initializing PRU instance ...
Did Map 0x30080000 len 0x2000 to 0x30080000 (dram0)
Did Map 0x30082000 len 0x2000 to 0x30082000 (dram1)
Did Map 0x300b4000 len 0x4000 to 0x300b4000 (iram0)
Did Map 0x300b8000 len 0x4000 to 0x300b8000 (iram1)
Did Map 0x30090000 len 0x10000 to 0x30090000 (shdram)
Did Map 0x300a2000 len 0x400 to 0x300a2000 (control0)
Did Map 0x300a4000 len 0x400 to 0x300a4000 (control1)
Did Map 0x300a0000 len 0x2000 to 0x300a0000 (intc)
Did Map 0x300a6000 len 0x2000 to 0x300a6000 (cfg)
Did Map 0x300a8000 len 0x2000 to 0x300a8000 (uart0)
Did Map 0x300ae000 len 0x2000 to 0x300ae000 (iep)
Did Map 0x300b0000 len 0x2000 to 0x300b0000 (ecap0)
Did Map 0x300b2000 len 0x400 to 0x300b2000 (mii_rt)
Did Map 0x300b2000 len 0x1c00 to 0x300b2000 (mdio)
Did Map 0x3008a000 len 0x2000 to 0x3008a000 (txPru0Iram)
Did Map 0x3008c000 len 0x2000 to 0x3008c000 (txPru1Iram)
Did Map 0x300a5000 len 0x100 to 0x300a5000 (txPru0CtlReg)
Did Map 0x300a5000 len 0x100 to 0x300a5000 (txPru1CtlReg)
Phy 15 : Disable RGMII mode
Phy 15 : Disable GBit ANEG
Phy 3 : Disable RGMII mode
Phy 3 : Disable GBit ANEG
Mode: MII
Thanks
Regards
Shine