Part Number: AM2634
Hello,
Regarding the training material: Introduction to Security in AM26x devices, it says "TI delivers an HSM Run Time firmware for HS-FS devices as a part of MCU_PLUS_SDK release."
Q1 : Is the TI delivered HSMRt the image contained in the file hsmRtImg.h in the MCU_SDK?
Q2: If so, I could not find any example projects which use this default HSMRt. The only examples I can find are in TIFS. However the TIFS documentation says "Support Device Type: HS-SE" for all the examples. So at the moment, I cannot find a project example that can be used on an HS-FS device with the default HSMRt. Does one exist please or do I have to create one from scratch?
Thank you.