This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: SPI Communication not working properly

Part Number: TM4C129ENCPDT

Hi,

I'm working with a TM4C129ENCPDT microcontroller connected to external flash memory via SPI2. The connections are correct since it works when I use TI-RTOS. However, when I configure it without TI-RTOS, I can send data but I'm unable to read from the flash; it always shows 0. Here's my code. Can you please help me resolve this issue?

#include "inc/hw_memmap.h"
#include "inc/hw_nvic.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/interrupt.h"
#include "driverlib/eeprom.h"
#include "inc/tm4c129encpdt.h"
#include "inc/hw_types.h"
#include "inc/hw_nvic.h"
#include "driverlib/gpio.h"
#include "inc/hw_memmap.h"
#include "inc/hw_flash.h"
#include "inc/hw_nvic.h"
#include "driverlib/ssi.h"

void main(void)

{

ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_OSC), 16000000);

SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);

//
// Enable clocks to GPIO Port D and configure pins as SSI
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);

GPIOPinConfigure(GPIO_PD3_SSI2CLK);
GPIOPinConfigure(GPIO_PD2_SSI2FSS);
GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);
GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);
GPIOPinTypeSSI(GPIO_PORTD_BASE, (GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3));


SSIConfigSetExpClk(SSI_BASE_ADDR, ui32SysClock, SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 1000000, 8);


// Enable the SSI module.

SSIEnable(SSI_BASE_ADDR);
SSIAdvModeSet(SSI_BASE_ADDR, SSI_ADV_MODE_READ_WRITE);
SSIAdvFrameHoldDisable(SSI_BASE_ADDR);

//
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
//
uint32_t junk;
while(SSIDataGetNonBlocking(SSI_BASE_ADDR, &junk));

readDeviceID();

}

uint8_t spiSendReceiveByte(const uint8_t dataTx)
{

// Remove any residual or old data from the receive FIFO
uint32_t junk;
while (SSIDataGetNonBlocking(SSI_BASE_ADDR, &junk));

// SSI TX & RX
uint8_t dataRx[2];
SSIDataPut(SSI_BASE_ADDR, (uint32_t) dataTx);


// Wait until the transmit buffer is not full
while(SSIBusy(SSI_BASE_ADDR));
SSIDataGet(SSI_BASE_ADDR, (uint32_t *) &dataRx);

return dataRx[0];
}

uint8_t readDeviceID(void)
{
uint8_t DeviceID = 0;

DeviceID = spiSendReceiveByte(W25Q32JV_COMMAND_JEDEC_ID);


return DeviceID;
}

Based on the provided code, it seems that SSIDataGet() is setting the dataRX to 0.

Do I need to use DMA for this? If so, could you please provide guidance on how to configure it?

Regards,

Sony

  • Hi,

    The connections are correct since it works when I use TI-RTOS

    TI-RTOS SPI example only uses the legacy SPI mode while you are using the Advance Mode. Why are you using the Advance. What is the slave device you have that requires you to use Advance Mode? I will suggest you use Legacy Mode first.

    Based on the provided code, it seems that SSIDataGet() is setting the dataRX to 0.

      When you said the received data is zero, have you looked at the scope to confirm that the slave is sending data on the RX pin or the slave is returning zero on the pin? Why don't you show the scope shot?

      Does your slave require SSI_FRF_MOTO_MODE_3? Please make sure both sides have the identical phase and polarity. 

      

  • Hi Sony,

      I have not heard back from you. I hope your problem is resolved. I will close the thread for now. If you have any update, you can write back to the post and the thread will automatically reopen to Open status.