Part Number: LP-AM243
Other Parts Discussed in Thread: UNIFLASH
Hi all TI experts,
I'm currently working with the LP-AM243 development board and I'm facing an issue while trying to flash my project's appimage into the LP board's flash memory. I've followed the development guide provided here for initializing the binary on the LP-AM243:
I've successfully built my project and used the debug mode to control the LP board. However, when I attempt to flash the appimage file into the flash memory, I encounter a problem.
After putting the LP board into UART boot mode, I observed the following information in the terminal:
Starting NULL Bootloader ...
DMSC Firmware Version 21.1.1--v2021.01a (Terrific Lla
DMSC Firmware revision 0x15
DMSC ABI revision 3.1
INFO: Bootloader_runCpu:147: CPU r5f1-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:147: CPU r5f1-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:147: CPU m4f0-0 is initialized to 400000000 Hz !!!
It seems like the LP board is still stuck in QSPI boot mode. I've attempted to execute the default_sbl_null.cfg using the following command after closing the UART port:
python3 uart_uniflash.py -p COM11 --cfg=sbl_prebuilt/am243x-lp/default_sbl_null.cfg
However, the progress remains at 0%, and after a few minutes, the script displays an error message: "No response or error response from EVM."
Could you please help me identify what I might be doing wrong?