This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: Recommended CCS version for Tivaware 2.2.0

Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: UNIFLASH,

Hi,

I just installed Tivaware 2.2.0.295. The enet_lwip builds with some warnings. But, what is the recommended CCS version for Tivaware 2.2.0.295? Also can I flash the program using Uniflash? Is the LM Flash Programmer still the tool for programming EK-TM4C1294XL?

-kel

  • Hi,

      I will suggest you use the latest CCS version CCS12 although earlier versions should also work.. 

      Yes, you can use Uniflash to flash the bootloader through the JTAG interface. You can use LM Flash Programmer tool to download your application through the Ethernet port.