Part Number: AM2634
Hi AM2634 champ
One customer wants to use Quad Read Mode (QSPI).
By the way, will there be an issue with QSPI/SPI0 performance if the 1.01k resistor is pull-down connected without DIP SW on the corresponding SOP 4pins?
I wonder if I have to apply a switch or buffer. Please recommend a suitable solution.


Thanks.
BR.Jack