This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: ADC Input Range Setting

Guru 10216 points

Part Number: AM2634

Hi AM2634 Champ

One customer is usinig the MCU internal vref as 1.8v. 

They want to change the input conversion range to 2.5V since their previous model uses 2.5V reference level.

Can you please check the followings?

-.How to set it in source code as an parameter
-.How to set up by entering External vref (what voltages should he enter ? 33/18*1.36 = 2.5V (2.493333) and 1.36V as External vref
- Is the conversion range fixed at 3.3V?

Thanks.

Regards, 

Jack