Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: The Vref of internal temperature sensor.

Part Number: MSPM0G3507

Hi champs,

In TRM we say TEMP_SENSE0.DATA is the ADC result code based on 12-bit mode and a 1.4-V reference.

My question is when we use internal temperature sensor, should we configure Vref to internal 1.4V reference for accuracy? Or we can configure Vref to other reference source, VDDA for example?

Regards,

Luke

  • Hi Luke,

    The TRM is wrong about the TEMP_SENSE0.DATA is the ADC result code based on 12-bit mode and a 1.4-V reference. It is actually using 3.3V VDDA as reference. 

    In the latest SDK, they all use 3.3V for calculation.

    Best regards,

    Cash Hao

  • Hi Cash,

    Another question is in the temperature sensor example project, we use _IQ15(3.45) to calculate Vtrim value, not use _IQ15(3.30), why?

    /*
    * Convert TEMP_SENSE0 result to equivalent voltage:
    * Vtrim = (3.3*(TEMP_SENSE0 -0.5))/(2^12)
    */

    qVTrim = _IQ15div(_IQ15mpy((_IQ15(DL_SYSCTL_getTempCalibrationConstant()) -
                      _IQ15(0.5)), _IQ15(3.45)), ((uint32_t)(1) << 27));

    Regards,

    Luke

  • Hi Luke,

    It should use the _IQ15(3.30) for Vtrim calculation. This will be fixed in further SDK.

    Best regards,

    Cash Hao