Other Parts Discussed in Thread: RM57L843, EK-TM4C1294XL
HI TI-Team,
I am newer to TIVA C Series Microcontrollers. We have chosen a TM4C1294KCPDTI3R IC for our project. We need a SPI, ADC, External Peripheral Interface,Ethernet(10/100)Mbps and less power consumption .I think this IC is suitable for our project or Suggest me an IC if not.
I have worked with RM57l843 microcontroller Ethernet data transmit but i have only achieved 4.9Mega Bytes per sec In datasheet 10/100Mbps(12.5 Mega Bytes per sec) I can't achieve 12.5MB/sec. This because why? We need to achieve 100Mbps data transmit in ethernet. Is it practically possible if not what are the reason cause for the losses. In this IC TM4C1294KCPDTI3R practically can we acheive 100Mbps?
And guide me to how start with this microcontroller.Where I find the example coding.
Thanks in advance,
Regards,
A. Ajith Kumar