This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: PWM/ Button pressing

Part Number: TM4C1294NCPDT

Hello everyone,

I am new to this but could you please help me with my code? I am trying to get the mic to turn the red and blu color on pwm on and off if a button is pressed but it's not working and I'm not sre why...here's the code:

Thank you so much <3

#include <stdint.h>
#include <stdbool.h>
#include <math.h>               // for sine wave
#include <stdio.h>              // for sprintf()
#include <inc/hw_memmap.h>
#include <inc/hw_types.h>
#include <inc/hw_gpio.h>
#include <driverlib/sysctl.h>
#include <driverlib/debug.h>
#include <driverlib/adc.h>
#include <driverlib/fpu.h>      // float support
#include <driverlib/gpio.h>
#include <driverlib/pwm.h>
#include <driverlib/pin_map.h>

#include "CFAF128128B0145T/CFAF128128B0145T.h"

// The error routine that is called if the driver library encounters an error.
#ifdef DEBUG
void __error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

#define PWM_FREQUENCY 100   // PWM frequency must be > 100 Hz for human eyes
#define APP_PI        3.1415926535897932384626433832795f
#define STEPS         256

int main(void)
{
    bool buttonPressed = false;  // Variable to track the button state

    volatile uint32_t ui32Load;         // PWM period
    volatile uint32_t ui32RedLevel;     // PWM duty cycle for red LED
    volatile uint32_t ui32GreenLevel;   // PWM duty cycle for green LED
    volatile uint32_t ui32BlueLevel;    // PWM duty cycle for blue LED
    volatile uint32_t ui32PWMClock;     // PWM clock frequency
    volatile uint32_t ui32SysClock;
    volatile uint32_t ui32Index;        // iteration counter
    float fAngle;
//  char strBuffer[30];                 // for sprintf()

    // Run from the PLL at 120 MHz.
    ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);

    // Display, Parameters
    CFAF128128B0145T_init(1, ui32SysClock, 20000000);

    // Write text
    CFAF128128B0145T_text(30, 60, "Hello World!", CFAF128128B0145T_color_white, CFAF128128B0145T_color_black, 1, 1);

    // Init Hardware
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);     // enable PWM0

    // Setup GPIOs, configure all three RGB LED pins to PWM
    GPIOPinTypeGPIOInput(GPIO_PORTJ_BASE, GPIO_PIN_0);
    GPIOPadConfigSet(GPIO_PORTJ_BASE, GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);

    GPIOPinTypePWM(GPIO_PORTG_BASE, GPIO_PIN_0);
    GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_2 | GPIO_PIN_3);
    GPIOPinConfigure(GPIO_PG0_M0PWM4);
    GPIOPinConfigure(GPIO_PF2_M0PWM2);
    GPIOPinConfigure(GPIO_PF3_M0PWM3);

    // Setup PWM clock
    PWMClockSet(PWM0_BASE, PWM_SYSCLK_DIV_64);           // 120MHz/64 = 1.875MHz

    // Calculate PWM load values
    ui32PWMClock = ui32SysClock/64;                      // 120 MHz/64
    ui32Load = (ui32PWMClock/PWM_FREQUENCY)-1;           // 1875000/100 = 18750

    // PWM Configuration (Red LED)
    PWMGenConfigure(PWM0_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN);
    PWMGenPeriodSet(PWM0_BASE, PWM_GEN_1, ui32Load);
    PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, 0);         // a starter for the load value
    PWMGenEnable(PWM0_BASE, PWM_GEN_1);
    PWMOutputState(PWM0_BASE, PWM_OUT_2_BIT, true);

    // PWM Configuration (Blue LED)
    PWMGenConfigure(PWM0_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN);
    PWMGenPeriodSet(PWM0_BASE, PWM_GEN_2, ui32Load);
    PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, 0);   // a starter for the load value
    PWMOutputState(PWM0_BASE, PWM_OUT_4_BIT, true); // switch on PWM output 4
    PWMGenEnable(PWM0_BASE, PWM_GEN_2);             // switch on generator 2


    ui32Index = 0;  // iteration counter

    while(1)
    {
        if(GPIOPinRead(GPIO_PORTJ_BASE, GPIO_PIN_0) == 0)
        {
            buttonPressed = true;
        }
        else {
            // Button is released, reset the buttonPressed flag
            buttonPressed = false;



            fAngle = ui32Index * (2.0f * APP_PI/STEPS);

        }
        if (buttonPressed){


            // Red LED
            PWMGenDisable(PWM0_BASE, PWM_GEN_2);
            ui32RedLevel = (uint32_t) (9370.0f * (1 + sinf(fAngle)));       // 18750/2 > 9370 to keep load value < max
            PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, ui32RedLevel +1);
    }
        else {
            // Blue LED
            PWMGenDisable(PWM0_BASE, PWM_GEN_1);
            ui32BlueLevel = (uint32_t) (9370.0f * (1 + sinf(fAngle+2*2.0f * APP_PI/3)));
            PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, ui32BlueLevel +1);

                }
        SysCtlDelay(ui32PWMClock / PWM_FREQUENCY);


    }
}

  • Hi,

    // PWM Configuration (Red LED)
        PWMGenConfigure(PWM0_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN);
        PWMGenPeriodSet(PWM0_BASE, PWM_GEN_1, ui32Load);
        PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, 0);         // a starter for the load value
        PWMGenEnable(PWM0_BASE, PWM_GEN_1);
        PWMOutputState(PWM0_BASE, PWM_OUT_2_BIT, true);

        // PWM Configuration (Blue LED)
        PWMGenConfigure(PWM0_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN);
        PWMGenPeriodSet(PWM0_BASE, PWM_GEN_2, ui32Load);
        PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, 0);   // a starter for the load value
        PWMOutputState(PWM0_BASE, PWM_OUT_4_BIT, true); // switch on PWM output 4
        PWMGenEnable(PWM0_BASE, PWM_GEN_2);             // switch on generator 2

    In the above code, per your comments, PWM_GEN_1 is used for RED LED and PWM_GEN_2 is used for Blue LED.

     However, in your below code, per your comments, Red LED is on PWM_GEN_2 and Blue LED is on PWM_GEN_1. At least based on your comments, they don't seem to be consistent with your PWM initialization. Regardless what the comments say, why do you try to disable PWM as in PWMGenDisable(PWM0_BASE, PWM_GEN_2) and             PWMGenDisable(PWM0_BASE, PWM_GEN_1)? You first disable PWM_GEN_2 and later change the PWM Pulse Width. When you disable PWM_GEN_2 the PWM generation will stop. 

            if (buttonPressed){


                // Red LED
                PWMGenDisable(PWM0_BASE, PWM_GEN_2);
                ui32RedLevel = (uint32_t) (9370.0f * (1 + sinf(fAngle)));       // 18750/2 > 9370 to keep load value < max
                PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, ui32RedLevel +1);
        }
            else {
                // Blue LED
                PWMGenDisable(PWM0_BASE, PWM_GEN_1);
                ui32BlueLevel = (uint32_t) (9370.0f * (1 + sinf(fAngle+2*2.0f * APP_PI/3)));
                PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, ui32BlueLevel +1);