Part Number: AM2634-Q1
Hi,
We’ve received a question about “EXT_REFCLK” from my customer. Could you confirm below ?
“EXT_REFCLK” is described as “up to 50MHz” in the Figure 6-18.Root Clocks in the TRM, but it is 100MHz in other descriptions in TRM.
Which is correct ? or is there some PLL between Root Clocks in Figure 6-18 and the function that uses "EXT_REFCLK" ?
Thanks and regards,
Hideaki