Part Number: TM4C1294KCPDT
- Can you repeat the same problem on all the boards you have?
ans -: yes all board have same problem
- Can you repeat the same problem when running the same code on a LaunchPad?
ans - pending due to launchPad availability in india .
- Check your nRST input to the MCU. Do you have proper pullup on this pin as recommended on the datasheet. Check the datasheet for recommendation.
ans:- yes nRST circuit is working good.
- Do you have stable power supply to the MCU on your board?
ans :- yes
- Do you generate a software reset somewhere inside your firmware?
ans :- I have checked in firmware there was no statement of rest .
- Do you have a Watchdog timer that might have expired and cause the reset to happen?
ans :- Currently disable watchdog timer .