Dear TI community and support staff,
We are considering the MSPM0L1305 MCU in one of our products.
Currently, we are investigating an in-system test procedure we need to run after PCBA of our product.
The MCU (master) is connected to an I2C sensor (slave). During the in-system test we want to electrically connect to the I2C-Bus via a needle adapter and directly communicate with the I2C interface (master) from our testing equipment. Therefore we have to disable the MCU's I2C pins / IO pins by setting them high-Z (so they cannot interfere).
To be independent of the firmware development, it would be most easy, to set the MCU into reset state by pulling NRST low via the same needle adapter during our testing procedure (several minutes in duration), during which the IO ports would be set high-Z.
Sadly, the datasheet is not clear about whether the pin driving mode is guaranteed to be reset while NRST is kept low for a long period of time: There might be a loop before entering the System Reset stage.
Could you please clarify?
Best regards
Markus Wegmann