Part Number: SYSCONFIG
Other Parts Discussed in Thread: TMDSCNCD263
Hello,
SETUP: I am using the TMDSCNCD263 control card, CCS 12.5, MCU+ SDK for AM263x 8.6.0.34, and SysConfig version 1.18.0.3266 (from thread AM2634: Sysconfig error - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums).
In SysConfig, I have a GPIO input set up. The only GPIO peripheral that it allows is GPIO0.

LARGER ISSUE: When I compile and run the code using the debugger, it gets stuck in HwiP_data_abort_handler_c(void).
I stepped through the code to see where it hangs up. The first function called in main() is System_init(); That is defined in ti_drivers_config.c from SysConfig. Within System_init(), it is fine until it calls GPIO_init(); inside the same file. Then it gets to GPIO_setDirMode(baseAddr, GPIO_ILLK_POLARITY_PIN, GPIO_ILLK_POLARITY_DIR); and hangs up.
LIKELY CAUSE: The baseAddr that is passed to this function is CSL_GPIO1_U_BASE (0x52001000ul). However, the GPIO examples provided in the SDK are given a base address of CSL_GPIO0_U_BASE (0x52000000ul).
A. Is my issue caused by an erroneous base address?
B. What is wrong with SysConfig that it is telling GPIO0 to have a base address for GPIO1? And I do I fix or work around it? I uninstalled CCS 12.4 this morning and installed the latest CCS 12.5 this morning.