Part Number: OCTVO-3P-AM335X
Our AM335x's sysboot[4:0] is set to 10011b.
When the power is repeatedly turned off and powered on, there will be occasional start-up from NANDI2C.The debug information shows boot device 6. The information as follow:

I measured the level of each pin of the sysboot with an oscilloscope, and it was all in line with the set value.
What will cause the system to boot from NANDI2C?
The system has printed the SPL information, does it mean that the NAND has been correctly recognized,Just failed when reading boot information from NAND?