This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 DCAN Performance Question

I've been having a problem with slow reading times from a DCAN on a TMS570 running at 160MHz.    VCLK and VCLKA are both at 80MHz.

 

 Two 32-bit reads from the IF3DATA and IF3DATB registers is taking 350ns.  I'm fairly sure it is not a pipeline issue because for testing purposes I'm doing 10 32-bit reads and increased it to 12 32-bit reads.  Going from 10 to 12 reads increased the time by 350ns.

 

Can anyone tell me why this might be?

 

Thanks,

JR Simma

Simma Software, Inc.

The J1939 Experts