Other Parts Discussed in Thread: MSPM0G3507,
Hello,
The datasheet Rev. B of the MSPM0G3507 explicitly mentions the MATHACL in the table in chapter 5 and also has an own section 8.22 on the topic.
The datasheet Rev. C of the MSPM0G1106 has not such entries regarding MATHACL. It only mentiones MATHACL in table 8-5 in Chapter 8.7.2. in the peripheral file map.
I am a bit unsure how to determine if the MSPM0G1106 has MATHACL available or not?
So 2 simple question:
- Has the MSPM0G1106 MATHACL?
- If yes on 1. is it exactly the same as for MSPM0G3507?
Best Regards
Marco