register address:0xFFF7B878
In TRM "Literature Number: SPNU489B", Page 1315, section 18.6.27.
In the description of this register, I have two questions:
1.It says this register can't be writtten by software application, and value is unchanged after reset. so, how to clear this register value ? if it clears 0x00000000, but 0x00000000 means the program field of first instruction have parity error, so, it should be cleard to which value ?
2.what does this sentence mean "This error address is frozen from being updated until it is read by the CPU. During emulation mode, this address is frozen even when read." ? and how to configure to enter emulation mode, except emulation mode, what modes it has and how to configure?
Thanks very much.