Part Number: TM4C1290NCPDT
All,
we're using LM Flash Programmer to upgrade FW and sometimes noticing, in an unpredictable manner and only on some PCs, the following:
- Sometimes no communication via USB
- In other cases the procedure doesn’t get to completion causing partial FW download
- PC: DELL Latitude 5500
- OS: Windows 10 Pro, versione 2004, build 19041.1415
- LM Flash Programmer - Build 1613
- Driver usb: Installed TivaWare_C_Series-2.2.0.295
- On prev versions needed to install a specific patch in folder “…TivaWare_C_Series-2.2.0.295\windows_drivers”, shoudn’t be the case now being same content already present confirmed?
Please see screenshots below for more details:
- Issues Encountered


Appearing as soon as program button is hit:

Thanks
Fabio