This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Position Manager Support

Guru 10186 points

Part Number: AM2434

Hi Am2x Champ

I'm guessing AM2x supports Position Manager, can I use the same as the C2000? If so, is there a CLB in AM2X?

Thanks.

Regards, 

Jack

  • Hi Jack,

    AM243x does not position manager like C2000, but it does support wide range of absolute encoder (up to 3 channels) protocols such as EnDat 2.2, Tawagama, Hyper-DSL, BISS-C and more to come using its powerful and flexible PRU-ICSSGs on chip.

    It also supports the SDFM (up to 9 channels) for current sensing using its PRU-ICSSG. 

    Best regards,

    Ming