This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Introduce benefits when using AM2x than C2000

Guru 10196 points

Part Number: AM2434

Hi AM2x Champ

We've heard that when using AM2x, communication function and power consumption are better than C2000,

so please introduce the detailed benefits.

Thanks.

Regards, 

Jack

  • Hi Jack,

    1. AM243x is able to support wide range of Industrial Communication Protocols such as EtherCAT, Ethernet/IP, Profinet, IO Link and more to come. Thanks to the powerful and flexible two PRU-ICSSG on chip.

    2. AM243x is able to support wide range of absolute encoder protocols such as EnDat 2.2, Tawagama, Hyper-DSL, BISS-C and more to come. Thanks to the powerful and flexible two PRU-ICSSG on chip.

    3. With four 800Mhz R5F cores and 2MB on chip memory, AM243x provides powerful real time control capability.

    4. The on-chip M4 core in the MCU domain makes it easy to implement the safety features.

    5. AM243x is able to support up to three servo motors on a single chip.

    Please check out our Motor Control SDK 9.0.0 for details. 

    Best regards,

    Ming