Part Number: MSPM0L1105
Hi.
Can we use the same pin to connect an slave IC with SPI interface and same bus to connect an another IC with I2C interface? I see within the datasheet that the pin configuration can be changed to use both type of interfaces and considering that both slave ICs have a chip select or can be turned off we could manage to communicate with each IC while the other is off.
Can the internal pull up resistor be used for the I2C? Or would you recommend an external pull resistor? I understand that the internal pull up resistor is a bit high for I2C, but I would like to know if it can be used or not.
Thanks