This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM-243x functions in FLASH

Hi,

I'm using the EVM-243x with TCP server example

I'd like to add functions in the FLASH.

Is it OSPI or QSPI device ? 

I have the following line in the linker FLASH     : ORIGIN = 0x60200000 , LENGTH = 0x100000

if I put a function in the FLASH - can it harm the boot loader ?

Which addresses of the FLASH are safe to use ? 

Thanks,

Eli