This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I have been looking at SysConfig files for both standalone and within CCS (in one of the examples) for the LP-MSPM0L1306.
However, I see quite a few differences between the two. Some differences I noticed are below.
Why are there these differences, and are there anymore that should be noted?
Does this have to do with SDK version?
Best regards,
Mari Tsunoda
Hi, Mari
You can see your syscfg version here:
The latest version is Version: 1.18.0.3266 Release date: 04 Oct 2023
On the "Reserve Peripherals" tab, there are more peripherals available
Check your version first. Here is the same.
In the standalone ver. it has this board view whereas CCS sysconfig ver. does not have this.
For hardware section and this question, please change the LaunchPad or device by click image button below:
Then click switch button to change LaunchPad or Board-None and Device-L1306.
Regards,
Helic
Hi Helic,
Thanks for your response.
I updated and re-checked everything, but still the same result for me. Do you have any differences between your CCS Sysconfig vs. standalone sysconfig or is this only an issue on my laptop?
Best,
Mari
Hi,
Here is the same of device L1306:
At sysconfig side, you need try this at start:
At CCS, right click project - properties - general - products:
Besides, we don't usually use reserve peripheral, software is more commonly used.
Regards,
Helic
Hi Helic,
Thanks for the super quick response. I see what you mean now.
Why is it that the ccs sysconfig opens up the 'board unselected' 'mspm0l1306' device for the example codes, when I choose for LP-MSPM0L1306, and not the LP specific sysconfig.
-Mari
Hi Helic,
Also, follow-up question: when should I pick the LP board specific sysconfig? or should I always just pick the board unselected option.
Best regards,
Mari Tsunoda
Hi,
It has a board view for easier hardware preview.
Actually, both board and device share the same MCU chip L1306.
follow-up question: when should I pick the LP board specific sysconfig? or should I always just pick the board unselected option.
There is no specific requirement to choose between them, because example code all use device selection, so
I usually use device-L306 instead of board LP-L1306.
Regards,
Helic
Hi Helic,
Thanks for your quick response.
In the standalone ver. it has this board view whereas CCS sysconfig ver. does not have this.
I understand this now.
So there is no code generation differences between the board vs device selection then?
Thanks,
Mari
Hi, Mari
So there is no code generation differences between the board vs device selection then?
Why not have a quick test for that?
Compare the file ti_msp_dl_config.x is OK.
A useful software will help you a lot: Scooter Software | Home of Beyond Compare
Regards,
Helic