Part Number: AM2732
Hi Experts
Could you pls help check what‘s the leakage current of GPIO when GPIo and pinmux is configured in high impedance state?
Thanks
Ken
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ken,
Apologies for the lack of reply here, I am currently out of office but I will be back and will look into this for you on 12/5.
Best Regards,
Ralph Jacobi
Hello Ken,
The GPIO when in high impedance state (receiver disabled, pull disabled) as a leakage current minimum of -18 uA and a leakage current maximum of 18 uA.
Here is a full table of leakage currents for the GPIO which will be added into the datasheet in the future:
| Parameter | Min | Typ | Max | Unit |
| Input Leakage Current, Receiver Disabled, Pull Disabled | -18 | 18 | uA | |
| Input Leakage Current, Receiver Disabled, Pullup Enabled | -243 | -100 | -19 | uA |
| Input Leakage Current, Receiver Disabled, Pulldown Enabled | 51 | 100 | 210 | uA |
Best Regards,
Ralph Jacobi