Part Number: TMDSEMU200-U
I have 2 x TMDSEMU200-U USB JTAG programmers that are connected to my PC. I need to be able to detect each one's USB Port uniquely. Each programmer will program a unique TI microprocessor. I see in device manager both programming modules listed as Ports but when I use LabVIEW to open a VISA session with them I am unable to. This would allow me to then query the port name of each program module uniquely.
Here are the details:
I’m unable to read the name of the device using NI-VISA commands to read out the name of the device its called in device manager. I just receive an error when trying to open a VISA session with the XDS200 programming module. Do I need to change any settings to make the name visible to be read?
NI LabVIEW VISA OPEN Error

Device Manager

Thanks so much!