This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0-G3507 / Can't connect anymore

Hello,

I'm not sure if our launchpad is broken, as I can't even connect anymore or factory reset...

"[ERROR] CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information."

Everytime I try to flash or mass erase or factory reset I'm getting this error.

Do you have any idea, if I can check anything anymore?

kind regards

Johannes