Hi team,
When I use sysconfig to set the configuration, the following alarms will appear in 2800157, but 280039 will not, how do I configure CCS so that all the configuration alarms of the 280039 can be popped up?
Thank you!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
When I use sysconfig to set the configuration, the following alarms will appear in 2800157, but 280039 will not, how do I configure CCS so that all the configuration alarms of the 280039 can be popped up?
Thank you!

Hi team, may I have your feedback? Thanks!
Hi,
If there is any out of range configuration, then the tool will pop up the warnings or error messages.
For F280015x devices, the max ADCCLK is 50 MHz and hence it is pointing out the message that the pre scalar needs to be corrected.
For F280039 device, the max ADCCLK is 60 MHz . If the configuration exceeds it , it will display the messages.
Best Regards
Siddharth