Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Hello,
In my customized board environment, UART framing errors rarely occur.
Therefore, I would like to check whether the ROSC settings are working properly.
Is there a way to check from register information?
SYSOSC is 4MHz.
Connect a 100kΩ (±0.1%) resistor to the external resistor and use ROSC.
The ClockTree settings in Sysconfig are as follows.
- Enable Frequency Correction Loop: Checked (Enabled)
- Enable Ext Reference Resistor (ROSC): Checked (Enabled)
- Disable SYSOSC: Not checked
CCS 12.5
Sysconfig version V1.18
mspm0_sdk_1_20_00_05