Other Parts Discussed in Thread: TMS470R1B1M
I'm trying to use TMS470R1B1M FLASH F05 0.36 API module files. I've added all the header files to my project but I'm unable to figure out how to use the.r79 files present in the API module. When I call the functions such as Flash_compact_b, Flash_Erase_b in my main program, IAR compiler just doesnt find those even though the prototype is declared in the headers. I understand that I've to somehow add/use the.r79 compiled files.
The error I get when I try to build without using the.r79 files is similar to - Error[Li005]: no definition for "Flash_Compact_B" [referenced from C:\Program Files (x86)\Texas Instruments\F05aFlashAPI_V.36\f05a v.36\Debug\Obj\main.o]
Could someone explain me how to use .79 files and just call the functions from the main?