Part Number: AM2432
AM243x can support etherCAT thanks to the PRU-iCSSG.
PRU-ICSSG can output the SYNC0 signal for synchronization with the EtherCAT master.
Which pin of the Sitara can be used to output the SYNC0 signal,
The purpose is to route it outside of the Sitara (on the PCB) and then route it back to the Sitara in order to synchronize the PWM the Sitara with the EtherCAT master.
Which pin of the AN2432 do you recommend to output the signal?
Thank you