This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507-Q1: Is there a automotive grade 64 PIN or 128 PIN MCU?

Part Number: MSPM0G3507-Q1

Hi Expert,

Please help with suggestions automotive grade MCU for TI part
MCU code flash(ROM) 512KB、RAM 64KB
The requirements for MCU IO are as follows:
GPIO *12~15:For Function Key、Led、Power enable、Camera indicator
INT*10~14:From ISP、ALS*2、Fault signal
PWM*2:For Backlight Driver
ADC*3:For Thermistor
I2C*2:For ISP、Bridge、ALS
CAN*1:must

Thanks

Daniel