Part Number: AM2431
TRM and datasheet reference debounce option on GPIO and EQEP pin.
I want to use the debounce option for PRU GPI mux mode = 1
Same pin can be system GPIO1_10 and EQEP0_A.

Question:
1. Does debounce function work with mux mode different to GPIO1_20 (mode 7) or EQEP0_A (mode 8)?
2. If so, which debounce settings apply, GPIO (25 MHz) or EQEP (250 MHz)?
BR,
Thomas