Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0714: TMS570LS0714PGE FREERTOS Problem

Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN

I am trying to use the FreeRTOS methods from Halcogen.

I am using Halcogen v04 07 01. I started with the project for Free RTOS : TMS570LS0714PGE_FREERTOS.

I have left settings related to RTOS unchanged. I am running the code based on the example_freeRTOSBlinky.c.

I have 2 tasks, both should toggle leds. The tasks are using vTaskDelay(xTimeInTicks);. 

I have started the scheduler.

The issue I see is that vTaskDelay is not working - it does not yield from the task. The high priority task runs all the time. The lower priority task never runs.

I think this is something to do with the interrupts for the RTI compare, or possibly SPV interrupt.

Please help.