Part Number: AM2634-Q1
Clock specifications (datasheet: SPRSP74 section 7.11.4.1.1 table)
Hi, please tell me about the following three things.
1. Fxtal is specified, but at what temperature?
2. Fxtal is from -50ppm to +50ppm. What problems will occur if this range is exceeded?
3. I want to use AM2634-Q1 in the range of -40 to +125℃.
However, I could not find a Crystal Oscillator that satisfies the tolerance range, temperature characteristics (-40 to +125℃), and aging (10 years) -50ppm to +50ppm in this range.
What type of crystal oscillator do you specifically think will be connected?
The following is a Japanese sentence for notes. Please do not worry.
クロックの仕様(データシート:SPRSP74 セクション7.11.4.1.1の表)について
次の3つのことについて教えてください
1. Fxtalが規定されているが何℃のときか?
2. Fxtalは-50ppmから+50ppmとなっている。この範囲を超えるとどのような不都合が起きるのか。
3. -40から+125℃の範囲でAM2634-Q1を使いたい。
しかし、この範囲で許容範囲、温度特性(-40から+125℃)、経年変化(10年)-50ppmから+50ppmを満たすCrystal Oscillatorが見つからない
どのような型名の水晶オシレータが接続されると具体的に考えているのか?