Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432E401Y: MSP-EXP432E401Y

Part Number: MSP-EXP432E401Y

What is the temperature range of the MSP-EXP432E401Y launch kit? I was wondering if it operates in the -20C - 85C temperature range.

  • Hi,

    We do not spec a temperature range for LaunchPads. They are evaluation modules and are intended to be used at room temperature. 

    Since these boards were designed to be used at room temperature for evaluation purposes, and not in an end product, we did not design or build the boards with extended temperature range in mind.  Even if all the components on the board are rated to a certain range, we do not guarantee the board or the manufacturing is rated to the same range.

    With that in mind, all we can recommend is that you use the LaunchPad at room temperature.