Part Number: AM2434
Hi all,
I have a few questions about the AM243x schematic, could you please help answering them?
- USB0_VBUS pin requires the VBUS voltage to be scaled down. My customer has trouble following the exact circuit in the LP, so they are using their own circuit. What's the requirement of the scaled signal? .Is there any scaling ratio my customer has to refer to?
- Datasheet mentioned connection requirements of MMC0 pins when MMC0 is not used, is this requirement applicable to MCC1 too? (and I2C0, I2C1 as well)
- There is a recommended crystal circuit in the data sheet, however, the LP uses a difference design. The crystal output connected to the device through a buffer. Customer followed the LP design but with CLK buffer removed, the crystal output is connected to the device through a 33Ohm-12pF RC filter, is this OK?
- There is a power-up sequence for this device, and MCU_PORz is the last to set high. Is it ok to simplify use RC to delay the MCU_PORz high signal (from 1v8 rail) to achieve this? If it is, what's the threshold of this pin?
Thanks,
Hang.