CORTEX_M0P: AutoRun: Target not run as breakpoint could not be set: _JobHardwareBreakpoint::ARM_DEBUG_V6M_bpu_add_breakpoint: FPB : All resources are in use.[22062]

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, RU
Breakpoint is not supported at some functions.
Also, there is breakpoint number limitation.
You can add "__BKPT(0);" after the line you want to add a breakpoint.
/* Default: LED1 and LED3 ON, LED2 OFF */
DL_GPIO_clearPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_2_PIN);
//Debug will stop at here:
__BKPT(0);
DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN |
GPIO_LEDS_USER_LED_3_PIN |
GPIO_LEDS_USER_TEST_PIN);
Regards,
Helic