Part Number: PROCESSOR-SDK-AM69A
I cannot even get "ti-processor-sdk-linux-j784s4-evm-09_00_00_06" setup completed. As a last reasorce, I create a VM runnung Ubuntu 22.04 instead of trying to run it on Ubuntu 24.04 or Debian 12.
Same song... the this setup crash again
Here are the last line before the crac:
System has required packages!
--------------------------------------------------------------------------------
Package verification and installation successfully completed
--------------------------------------------------------------------------------
Do you wish to run nfs setup (Press (Y) to run, (n) to skip) ? y
/bin/sh: warning: setlocale: LC_ALL: cannot change locale (en_US.UTF-8)
--------------------------------------------------------------------------------
In which directory do you want to install the target filesystem?(if this directory does not exist it will be created)
[ /targetNFS ]
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will extract the target filesystem to /targetNFS
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue
xz: (stdin): Compressed data is corrupt
tar: Unexpected EOF in archive
tar: Unexpected EOF in archive
tar: Error is not recoverable: exiting now
Failed setup, aborting..
Failed setup, aborting..
What is wrong whit this setup?